Technical FAQs

Ask a Question

Is there an automated marking system available for the AB1 terminal blocks?

Yes. There is a plotter system and software available. The catalog numbers are: AB1MARKSOFT for the software. AB1MARKSYS1 and AB1MARKSYS2 are the two options for the plotter.


CTA-ID : 2028477
Was this helpful?
What can we do to improve the information ?