Technical FAQs

Ask a Question

Does the SU3040D400CB contain a bypass on the meter socket?

Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices

Cause:
Bypass Type

Resolution:
Yes, a manual link +bypass is supplied factory installed on this device. The manual link bypass provides the same bypass function as a test block bypass.


CTA-ID : 2028366
Was this helpful?
What can we do to improve the information ?