Technical FAQs

Ask a Question

Are QO Load Centers Suitable for Use as Service Equipment?

Issue:
Application

Product Line:
QO Load Center

Cause:
Application confirmation

Resolution:
With the exception of the catalog numbers shown below, all QO load centers are marked as Suitable for use as service equipment if equipped with integral main breaker, or when not more than six disconnecting means are provided and the panelboard is not used as a lighting and appliance branch circuit panelboard. 
Refer to the load center wiring diagram for specifics to suitability for use as service equipment and install per the National Electrical Code (NEC).
EXCEPTIONS: QO2L30S, QO2L30TTS, QO24L50TTS, QO24L70TS, QO35FM30TTF, QO35M30TTS, QO48M30DSGP


CTA-ID : 2028154
Was this helpful?
What can we do to improve the information ?