Technical FAQs

Ask a Question

How are the terminals marked on a 9013 pressure switch?<br />

There are four terminals all in a line (2 poles). The two outside terminals are marked LINE, the two inside terminals are marked LOAD.


CTA-ID : 2028302
Was this helpful?
What can we do to improve the information ?