Technical FAQs

Ask a Question

What is the Short Circuit Current Rating (SCCR) for the RC2M200S Combination Service Entrance Device?

The SCCR for this device is 22,000 RMS Symmetrical Amperes at 120/240Vac maximum when using QOM2-VH and QO-VH main breakers. If a QOM2-VH and a standard QO main breaker are used, the SCCR is 10,000 RMS Symmetrical Amperes at 120/240Vac maximum.


CTA-ID : 2028233
Was this helpful?
What can we do to improve the information ?