Technical FAQs

Ask a Question

What is the temperature rating on the lugs of Main Lug Only I-Line panels?

I-Line lugs are rated at 75 degrees C.


CTA-ID : 2028438
Was this helpful?
What can we do to improve the information ?