Technical FAQs

Ask a Question

Does the UT6R2392TU Horizontal Ganged Meter Socket have a common neutral bus for all six meters?

Yes, the UT6R2392TU does have a common neutral bus for all meters. There is a utility section in the center of the device which includes lugs for the incoming phases, neutral and service ground. Horizontal bussing feeds the six meter sockets and each socket provides lugs to feed the phase and neutral conductors to the dwelling units.

CTA-ID : 2028347
Was this helpful?
What can we do to improve the information ?