Technical FAQs

Ask a Question

What is the Short Circuit Current Rating (SCCR) for the QC12L200CH Combination Service Entrance Device?

The SCCR for this device is 22,000 RMS Symmetrical Amperes at 120/240Vac maximum when using QO-VH main breakers. If standard QO main breakers are used, the SCCR is 10,000 RMS Symmetrical Amperes at 120/240Vac maximum.


CTA-ID : 2028237
Was this helpful?
What can we do to improve the information ?