Technical FAQs

Ask a Question

What is the terminal lug data for a SO1020M100S Combination Service Entrance Device?

The main phase and neutral lugs accept a #6 - #1 AWG copper or aluminum conductor. The service ground lug accepts a #14 - #4 AWG copper or a #12 - #4 AWG aluminum conductor.

CTA-ID : 2028115
Was this helpful?
What can we do to improve the information ?