Technical FAQs

Ask a Question

Do MP Meter-Pak devices include a separate neutral bonding strap?

No, there is no separate bonding strap needed in the MP devices. This is because the neutral is already bonded from the factory. This means that the MP devices are suitable ONLY as Service Equipment.


CTA-ID : 2028430
Was this helpful?
What can we do to improve the information ?