Technical FAQs

Ask a Question

Is the S29354 mechanical interlock available for the Type H I -Line circuit breaker?

The part number S29354 is not available for the I-Line type H circuit breaker. Because of the size difference between the unit breaker and the I-Line breaker this interlock does not fit.

CTA-ID : 2028284
Was this helpful?
What can we do to improve the information ?