Technical FAQs

Ask a Question

Which button is maintained and which button is momentary on a 9001KXRF type operator?<br />

The top is momentary and the bottom is maintained. This is the standard start stop arrangement.



CTA-ID : 2028279
Was this helpful?
What can we do to improve the information ?