Technical FAQs

Ask a Question

Can Modbus connection be converted to Ethernet to communicate with the Altivar 58?

Yes. However, it is more common to use the Altivar 58 Ethernet Modbus® TCP/IP Communication Option (VW3A58310U) for the Altivar 58 drive.

CTA-ID : 9549
Was this helpful?
What can we do to improve the information ?