Technical FAQs

Ask a Question

Is a pedestal available for use with a PAK10CTG Servicepak Power Outlet Panel?

A pedestal for use with this device is not available. However, you may want to consider using a PAK11PG, which is provided with an integral pedestal. The PAK11PG is not an exact electrical equivalent to the PAK10CTG, as it is supplied with (2) NEMA 5-20R receptacles, both fed by QO120GFI circuit breakers, rather than (1) NEMA 5-20R receptacle.

CTA-ID : 2028737
Was this helpful?
What can we do to improve the information ?