Technical FAQs

Ask a Question

What is the main wire size for a PAK10C1?

This main terminals on this device will accept (1) #14 - 6 AWG CU or (1) #12 - 6 AWG AL per phase and neutral.


CTA-ID : 2028677
Was this helpful?
What can we do to improve the information ?