Technical FAQs

Ask a Question

What receptacles are provided in a PAK1004CGFI Servicepak Power Outlet Panel?

This device is provided with (1) NEMA 5-20R receptacle (20A, 125V, 2W and Grd) and (2) NEMA 14-50R receptacles (50A, 125/250V, 3W and Grd).


CTA-ID : 2028631
Was this helpful?
What can we do to improve the information ?