Technical FAQs

Ask a Question

What receptacles are provided in a PAK76CGFI Servicepak Power Outlet Panel?

This device is provided with (2) NEMA 5-20R receptacles (20A, 125V, 2W and Grd) and (1) NEMA 14-50R receptacle (50A, 125/250V, 3W and Grd).


CTA-ID : 2028630
Was this helpful?
What can we do to improve the information ?