Technical FAQs

Ask a Question

What receptacles are provided in a PAK61CTG Servicepak Power Outlet Panel?

This device is provided with (1) NEMA 5-20R receptacle (20A, 125V, 2W and Grd) and (2) ANSI #73.13 receptacles (30A, 125V, 2W and Grd).


CTA-ID : 2028633
Was this helpful?
What can we do to improve the information ?