Technical FAQs

Ask a Question

What type of mains are provided on a HOM1632U200TC load center?

This device is a ``Universal Mains`` load center, which is not initially supplied with a main device. A Main Breaker Kit or a Main Lugs Kit can be field installed as the application may require. To use as a Main Lugs load center, order and field install a QOL225. To use as a Main Breaker load center, order and field install a QOM2-VH Main Breaker Kit, 200A maximum. Catalog numbers for available Main Breaker Kits would be QOM2100VH (100A), QOM2125VH (125A), QOM2150VH (150A), QOM2175VH (175A) or QOM2200VH (200A).


CTA-ID : 2028590
Was this helpful?
What can we do to improve the information ?