Technical FAQs

Ask a Question

Other than through the Keypad or PowerSuite, is it possible to change the IP address of the Ethernet card for an Altivar 58 drive?

The IP address can only be changed via the keypad in menu 8 or through PowerSuite.
On Ethernet cards V1.2 or greater (introduced in mid 2004) the cards can be identified by device name using FDR (Faulty Device Replacement).
This will automatically assign the IP address, Subnet mask and Gateway when used with PLCs equipped with FDR capability.


CTA-ID : 2009819
Was this helpful?
What can we do to improve the information ?