Technical FAQs

Ask a Question

On an EZM32000CB1600, will the device`s nameplate read 2000A Max or 1600A Max?

The nameplate will read 2000A Maximum.


CTA-ID : 2028542
Was this helpful?
What can we do to improve the information ?