Technical FAQs

Ask a Question

What horsepower range of 3 phase motors can be controlled by a ATV58 single phase 208/230vac input Drive?

The ATV58 can go up to 30hp 208/230vac Single Phase input with 3 phase output for Variable Torque Low Noise applications.
All ATV58 single phase input drives over 3hp must have a 3% (Minimum) line reactor.
Also, note the proper selection and rating of the drives as shown in the installation guide.


CTA-ID : 2008810
Was this helpful?
What can we do to improve the information ?