Technical FAQs

Ask a Question

Can an analog output on the ATV58 be set to Motor Current?

Yes. In menu 5 (I-O menu) the analog output can be set for motor current (OCr).
Drives with V5.1 or higher version control boards have analog output AO1. If an option card is installed there may be additional outputs available.
They are both programmable for any of the available settings, including motor current.
AO and AO1 are 4-20 mA or 0-20 mA outputs.
See the Alitvar 58 Keypad Display instruction bulletin for details.

CTA-ID : 2010374
Was this helpful?
What can we do to improve the information ?