Technical FAQs

Ask a Question

Is there a defeat mechanism for the door interlock on a QMB type fusible switch QMB324, series D2 switch and how is it operated?

Yes. There is a rectangular shaped hole on the front, next to the handle. A flat blade screwdriver is used to insert into the hole, and it blocks the mechanism enough to open the door.


CTA-ID : 2028549
Was this helpful?
What can we do to improve the information ?