Technical FAQs

Ask a Question

Is a QO816L100F load center UL listed for a service entrance equipment application?

Yes, this device is UL listed as ``Suitable for use as service equipment``. The loadcenter can be applied as service entrance equipment in two different ways; 1) as a multiple main disconnect panel, and 2) as a single main disconnect panel when equipped with a back fed main breaker. When applied as a multiple main device, a maximum of six branch mounted main breakers can be used. When applied as a single main device, a PK2MB retaining kit is required for the single back fed main breaker.

CTA-ID : 2028525
Was this helpful?
What can we do to improve the information ?