Technical FAQs

Ask a Question

How can the firmware version of the Altivar 58 keypad be determined?

The firmware of the keypad is located on the back of that keypad itself.
On the back of keypad toward the top there is a white sticker with a bar code and some numbers. The revision number is on that sticker.
Example: V5.3 IE 32

CTA-ID : 2008802
Was this helpful?
What can we do to improve the information ?