Technical FAQs

Ask a Question

Why does the reset button not reset the switch for cable pull part number XY2CH13250H7?

The cable must be tight in order for the switch to be reset. If the cable is loose the reset button will not reset the switch. In addition, the cam followeer must be centered on the cam and not riding up on either shoulder.

CTA-ID : 2028600
Was this helpful?
What can we do to improve the information ?