Technical FAQs

Ask a Question

With the ATV58, can an I-O card be used at the same time as a serial communication card?

No. It is only possible to have one option card installed on an Altivar 58 drive at any one time.

CTA-ID : 2012743
Was this helpful?
What can we do to improve the information ?