Technical FAQs

Ask a Question

Does freewheel or fast stop still function when an Altivar 58 is running by means of a serial communications network?

Yes. Operation of a logic input programmed for freewheel stop (nSt) and Fast Stop (FSt) will cause the drive to stop running.
This is true even if there is no forced local.

CTA-ID : 2012110
Was this helpful?
What can we do to improve the information ?