Technical FAQs

Ask a Question

Does the 115VAC option card (VW3A58275U) work when using a conduit entrace kit with an Altivar 58 drive?

Yes. There is enough space for the 115 VAC option card to be installed with or without a conduit kit installed.

CTA-ID : 2009673
Was this helpful?
What can we do to improve the information ?