Technical FAQs

Ask a Question

Will a MicroLogic breaker operate properly using only 1 of the 3 available poles?

These breakers will work properly if only one pole is used. The indicating circuitry, such as the LCD screen, etc. may require the pole to loaded up to approximately 20% of full breaker capacity.


CTA-ID : 2027771
Was this helpful?
What can we do to improve the information ?