Technical FAQs

Ask a Question

We are installing a Ventilated Transformer. Can we use 105 C wire routed over the top of the coils inside the enclosure?

Internal conductor routing

Product Line:
LV Transformers

Applies to Ventilated Transformers by SquareD/Schneider Electric

Conductor wiring on Ventilated Transformers must be oriented from the bottom of the internal terminal strip. 


No. There is a label with arrows fixed to the inside and outside the enclosure side panel. All leads must be brought into the wiring compartment below the arrow, no matter what the wire temperature rating. Routing wire over the coil presents a safety hazaard and should never be considered.

CTA-ID : 2027504
Was this helpful?
What can we do to improve the information ?