Technical FAQs

Ask a Question

Can the UT4R2352T horizontal ganged meter socket be obtained with studs only instead of mechanical lugs?

This horizontally ganged meter socket device is provided with mechanical lugs to accept #1/0 AWG - 500 MCM conductors per phase and neutral. Studs only are not available on this device.


CTA-ID : 2027502
Was this helpful?
What can we do to improve the information ?