Technical FAQs

Ask a Question

Can the SE mechanism or main spring be repaired or replaced?

The SE mechanism is not repairable. Parts are not available, and there are no procedures or provisions within the company for working on it--even at the factory. If the mechanism is bad, a new breaker is required.

CTA-ID : 2027497
Was this helpful?
What can we do to improve the information ?