Technical FAQs

Ask a Question

Are there any restrictions with regards to the ampacity of circuit breakers used in a QO35FM30TTS loadcenter?

Yes, the branch breakers are restricted to 20 ampere maximum, single pole QO or QOT breakers. The main breaker is restricted to a 30 ampere maximum, single pole QO breaker.


CTA-ID : 2027999
Was this helpful?
What can we do to improve the information ?