Technical FAQs

Ask a Question

What are the new standard depths for HVL/cc rear extensions?

16.75``, 24.0`` and 30.0``
16.75`` is for lineup with 54`` deep transformers.
These can be used with 14.75``, 20.0`` and 29.50`` wide sections. Both indoor and outdoor.


CTA-ID : 2027991
Was this helpful?
What can we do to improve the information ?