Technical FAQs

Ask a Question

Can 9012GAW5 be used on steam?

Yes, use a 9049A7A steam capillary with it. Pressure restriction is 250PSIG. Higher pressures can cause superheated steam to overtemp the switch components. Although we formerly offered this product, the 9049A7A steam capillary is obsolete and no longer available. Users may construct one themselves, by creating a capillary tube coil 10 feet in length, attaching one end through a flared fitting to the pressure switch port, and the other to the monitoring point on the steam system. The 10 foot coiled tube acts as a condensor, cooling the steam to an acceptable temperature level.

CTA-ID : 2027984
Was this helpful?
What can we do to improve the information ?