Technical FAQs

Ask a Question

When mounted on a wall, what is dimension of the space between the wall and the back of the enclosure of an EZM device?

The dimension from the wall to the back of the EZM device is approximately 0.31inches.


CTA-ID : 2027737
Was this helpful?
What can we do to improve the information ?