Technical FAQs

Ask a Question

What does the R suffix indicate in the catalog number QMB361TWR?

Issue:
What is the QMB361TWR?

Product Line:
QMB panelboard, switchboard with QMB distribution.

Cause:
Product features.

Resolution:
The R suffix indicates that Class R fuse clips are factory installed into the QMB361TW switch. The QMB361TW is a twin 3 Pole, 30A, 600V switch. The Class R fuse clips will be provided on both switches in the unit. 


CTA-ID : 2027488

Was this helpful?
What can we do to improve the information ?