Technical FAQs

Ask a Question

Is there a NEMA 4 boot, which can be, used with the Class 9066 Type RA__ or Type RB NEMA 1 and NEMA 12 external reset mechanisms?

Yes, order 9066W1.


CTA-ID : 2027484
Was this helpful?
What can we do to improve the information ?