Technical FAQs

Ask a Question

What is the terminal lug data for a QU816D400SL?

The main service ground lug accepts a #4 AWG - 250 KCMIL conductor. The main phase and neutral lugs are not provided with this CSED device. This device is supplied with line and neutral lug landing pads for use with field installed compression or mechanical type lugs. For mechanical lugs, use lug kit CMELK4. This lug kit consists of four lugs, each lug capable of terminating (1) #2 AWG - 600 kcmil aluminum or copper conductor. Only three of the four lugs provided in the CMELK4 kit will be used. Optional mechanical lugs listed on the device wiring diagram include: ILSCO TA-600-2N (#2 AWG - 600 kcmil aluminum or copper), ILSCO TA-800-2N (300 - 800 kcmil aluminum or copper, Anderson L1D2-350 (#6 AWG - 350 kcmil aluminum or copper) or Anderson L1D2-800 (300 - 800 kcmil aluminum or copper). Optional Anderson Compression lugs: Anderson VHCL-600-12BN (250 - 600 kcmil copper) or Anderson VHCL-750-12BN (500 - 750 kcmil copper).

CTA-ID : 2027976
Was this helpful?
What can we do to improve the information ?