Technical FAQs

Ask a Question

Can an NQOD424M100 main breaker panel be converted to a main lug type panel?

Issue:
Can an NQOD424M100 Main breaker panel be converted to a Main Lug type Panelboard?

Product Line:
NQOD Panelboard

Environment:
Installed Main breaker

Cause:
Main breaker removal

Resolution:
 It is possible to substitute a sub feed lug kit QOB3125SL, for the Main breaker. However, the Panelboard labeling states Maximum ampacity 100A due to the Main breaker amperage and the Sub feed lug kit is rated for 125A, so there could be an inspection issue.
Was this helpful?
What can we do to improve the information ?