Technical FAQs

Ask a Question

Will a 2-pole HJA breaker fit in the same space as a 2-pole FC I-Line breaker?

Yes, the HJA will occupy 4.5 inches of mounting height which is the same as the FC 2 pole breaker. The HLA 2 pole breaker is also 4.5 inches of mounting height.

CTA-ID : 2027466
Was this helpful?
What can we do to improve the information ?