Technical FAQs

Ask a Question

What is the terminal lug data for a RU3040D400CK?

The main service ground lug accepts a #4 AWG - 250 KCMIL conductor. The main phase and neutral lugs are not provided with this CSED device. This device is supplied with line and neutral lug landing pads for use with field installed Anderson Compression lugs. Anderson Compression lugs listed on the device wiring diagram include: Anderson VHCL-600-12BN (250 - 600 kcmil copper) or Anderson VHCL-750-12BN (500 - 750 kcmil copper).

CTA-ID : 2027967
Was this helpful?
What can we do to improve the information ?