Technical FAQs

Ask a Question

Can a QBL22125 circuit breaker be used in place of a QBP22125?

No. The lugs cannot be removed from the on end of the QBL22125 to make it function in place of a QBP22125. Q frame breakers have fixed lugs which cannot be replaced or changed.

CTA-ID : 2027707
Was this helpful?
What can we do to improve the information ?