Technical FAQs

Ask a Question

How is the RZD603, Z-divider, installed?

The Z-divider can be secured to the bottom of the duct by welding, pop-riveting or screws depending on the preference of the installer. After that is done, the adjustment for divider height should be locked into place by tack welding so the divider provides additional support to the covers.

CTA-ID : 2027451
Was this helpful?
What can we do to improve the information ?