Technical FAQs

Ask a Question

What are the dimensions for potentiometer face plate number # 6517512701 ?

Issue:
What  are the dimensions for potentiometer face plate number # 6517512701 ?

Product Line:
22mm Push Button

Environment:
XB4/XB5 22mm Push Buttons      

Cause:
Clarify if the legend plate will fit for application                  

Resolution:                                                                 
40mm wide at top and bottom , 44mm wide in the center and 44mm high
Was this helpful?
What can we do to improve the information ?