Technical FAQs

Ask a Question

What is the heat dissipation for an ATS01N244LY?

22 Watts at full load at the end of starting.
268 Watts during starting and stopping at 3 times the rated operating current.

Reviewed 10/2011


CTA-ID : 2027673
Was this helpful?
What can we do to improve the information ?