Technical FAQs

Ask a Question

Can you use a Altistart ATS46 to replace an autotransformer type soft starter?

In many applications that have autotransformer soft starters it is possible to use a solid state soft starter such as an ATS46. It is important to consider the number of starts per hour as well as the amps required to start the load. Sometimes the autotransformer type soft starters are preferred in heavy duty applications where the duty cycle is high.

CTA-ID : 7432
Was this helpful?
What can we do to improve the information ?