Technical FAQs

Ask a Question

Why do we require fuse on the line side of an Altivar ATV66?

This drive was tested and UL rated to have input line fuses to protect against an internal short circuit on the DC bus.



CTA-ID : 6728
Was this helpful?
What can we do to improve the information ?